Terms of Trade
Lapp Connecto complies with the NL09, NL10 or NLM10 general sales conditions with the following changes and/or additions:
20.3.2024
No Re-Export to Russian Federation
- The [Buyer] shall not sell, export or re-export, directly or indirectly, to the Russian Federation or for use in the Russian Federation any goods supplied under or in connection with this Agreement that fall under the scope of Article 12g of Council Regulation (EU) No 833/2014.
- The [Buyer] shall undertake its best efforts to ensure that the purpose of paragraph (1) is not frustrated by any third parties further down the commercial chain, including by possible resellers.
- The [Buyer] shall set up and maintain an adequate monitoring mechanism to detect conduct by any third parties further down the commercial chain, including by possible resellers, that would frustrate the purpose of paragraph (1).
- Any culpable violation of paragraphs (1), (2) or (3) shall constitute a material breach of an essential element of this Agreement, and the [Exporter/Seller] shall be entitled to seek appropriate remedies, including, but not limited to:
- immediate termination of this Agreement for just cause; and
- a penalty of 100% of the total value of the net value of the respective order whereas the [Buyer] is expressly permitted to prove that a damage has either not occurred or is substantially less than the penalty.
- The [Buyer] shall immediately inform the [Exporter/Seller] about any problems in applying paragraphs (1), (2) or (3), including any relevant activities by third parties that could frustrate the purpose of paragraph (1). The [Buyer] shall make available to the [Exporter/Seller] information concerning compliance with the obligations under paragraph (1), (2) and (3) within two weeks of the simple request of such information.
More detailed documents will be sent upon request, please contact your contact person.